FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Encoder feedback speed accuracy
FAQ
Encoder feedback speed accuracy
How high is the accuracy for the inverter command output when using encoder feedback control and vector control of the FR-A5AP (FR-A520)?
- Category :
Answer
The speed variation rate is as follows:
- Encoder feedback control: ±0.2% - Vector control: ±0.02% (mentioned in FR-A5AP Instruction Manual)
- Encoder feedback control: ±0.2% - Vector control: ±0.02% (mentioned in FR-A5AP Instruction Manual)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-A500