FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Monitor output
FAQ
Monitor output
Can I input the monitor output from (the terminals FM and SD of) the inverter A024 to the analog input of the programmable controller (for example, A68AD)?
- Category :
Answer
The FM output is the 1440 Hz, 1 mA pulse train output at full scale.
You can input to the programmable controller if it has a pulse train input. A68AD does not have the pulse train input.
You can input to the programmable controller if it has a pulse train input. A68AD does not have the pulse train input.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024