FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Countermeasure against harmonics
FAQ
Countermeasure against harmonics
I am planning to insert DCL to suppress harmonics for the inverter capacity of 0.4K to 55K. Should I also insert ACL?
- Category :
Answer
Perform calculation given in the harmonic suppression guidelines, and if the limit value is exceeded, you may also need to insert the ACL.
Note that you cannot obtain a double harmonics suppression effect by inserting both DCL and ACL.
For harmonics reduction rate, refer to the harmonic suppression guidelines.
Note that you cannot obtain a double harmonics suppression effect by inserting both DCL and ACL.
For harmonics reduction rate, refer to the harmonic suppression guidelines.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power factor improving reactor
- Series
- Option