FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Parameter No.79 (Operation mode)
FAQ
Parameter No.79 (Operation mode)
I use the inverter FR-E500 and set Pr.79 (Operation mode) to "3" to use the potentiometer on the inverter.
When the multi-speed command is input, multi-speed operation is enabled. Can I cancel this?
When the multi-speed command is input, multi-speed operation is enabled. Can I cancel this?
- Category :
Answer
You cannot cancel multi-speed command input.
When the multi-speed command is input from the terminal, you cannot use the potentiometer.
Use the inverter so that the multi-command is not input (not turned ON) from the terminal.
When the multi-speed command is input from the terminal, you cannot use the potentiometer.
Use the inverter so that the multi-command is not input (not turned ON) from the terminal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500