FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Sensitivity current of earth leakage circuit breaker
FAQ
Sensitivity current of earth leakage circuit breaker
The earth leakage circuit breaker NV-FA series is available for the sensitivity current 30 mA only. Can I install it on the inverter input side?
- Category :
Answer
The rated sensitivity current of the earth leakage circuit breaker can be calculated using the following equation.
If the result is 30 mA or less, the NV-FA series can be used.
(If not, you need to use a NV type with a higher rated sensitivity current.)
If the result is 30 mA or less, the NV-FA series can be used.
(If not, you need to use a NV type with a higher rated sensitivity current.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Earth leakage circuit breaker
- Series
- Peripheral devices