FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Analog signal resolution
FAQ
Analog signal resolution
How are the internal processing speed and analog input signal resolution of the FR-A500 series compared with the servo MR-H series amplifier?
What about the FR-E500 series?
What about the FR-E500 series?
- Category :
Answer
The internal processing speed is not published.
The analog input specifications are as follows:
FR-A500???1/4000FR-E500???1/1000MR-H???1/4000
The analog input specifications are as follows:
FR-A500???1/4000FR-E500???1/1000MR-H???1/4000
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500, FR-A500