FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Inverter selection when multiple inverters are to be connected
FAQ
Inverter selection when multiple inverters are to be connected
When multiple inverters are to be connected, how should I choose them?
- Category :
Answer
Be sure to use a high power factor converter with the capacity higher than the total capacity of the inverters connected. (Note: One or more of the inverters must have capacity more than half of the high power factor converter.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option