FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > System configuration
FAQ
System configuration
What is the system configuration?
- Category :
Answer
The whole system consists of the power supply, molded case circuit breaker, high power factor converter, inverter, and motor. The high power factor converter system consists of the reactor L1, outside box, reactor L2, and converter (FR-HC). An installation space approximately 2.5 times of the inverter itself is required. Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option