FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > DIN rail installation
FAQ
DIN rail installation
Is the DIN rail installation available?
- Category :
Answer
Unit type: SC-A□□U can be installed on the DIN rail.
Box type: SC-A□□B cannot be installed on the DIN rail.
Box type: SC-A□□B cannot be installed on the DIN rail.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A