FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Difference from general-purpose inverter
FAQ
Difference from general-purpose inverter
What are the differences between the general-purpose inverter and inverter speed controller?
- Category :
Answer
In general, both are inverters using the same control method, however, the inverter speed controller limits functions compared with the general-purpose inverter to implement variable speed operation easily and prioritizes the size, usability, and cost.
Note that while the general-purpose inverter's control circuit terminals are insulated from the main circuit terminals to which high voltage is applied, those of the speed controller are not insulated and you should be very careful about this.
Note that while the general-purpose inverter's control circuit terminals are insulated from the main circuit terminals to which high voltage is applied, those of the speed controller are not insulated and you should be very careful about this.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A