FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Engineering Software > What type of personal computer is required?
FAQ
What type of personal computer is required?
What type of personal computer is required?
- Category :
Answer
The PC platform can be PC98 or DOS/V as far as Windows 3.1 or Windows 95 runs smoothly, with free space of 1 MB or more on the hard disk, and memory (RAM) 1 MB or more.
To install the software, one or more 3.5-inch floppy disk drive are required.
A mouse and serial port are also required.
To install the software, one or more 3.5-inch floppy disk drive are required.
A mouse and serial port are also required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter communication software
- Series
- Engineering software