FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Terminal CS
FAQ
Terminal CS
I once used the FR-A500 series.
At that time, the terminals CS and SD were short-circuited for automatic restart after instantaneous power failure, does the FR-E700 series have the terminal CS?
At that time, the terminals CS and SD were short-circuited for automatic restart after instantaneous power failure, does the FR-E700 series have the terminal CS?
- Category :
Answer
FR-E700, D700, and F700PJ do not have the terminal CS and you can only control automatic restart by setting Pr.57 (Restart coasting time).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ