FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Device Net classes
FAQ
Device Net classes
I do not understand the meanings of some terms used in the Instruction Manual of the Device Net.
1. Class
2. Instance
3. Attribute
I often see these three terms.
1. Class
2. Instance
3. Attribute
I often see these three terms.
- Category :
Answer
Class, instance, and attribute represents different grouping of objects.
Comparing object grouping to a mailing address, they can be considered as follows:
State (= class), city (=instance), and town (= attribute)
For inverter control, available parameters and operation commands are grouped into classes.
Comparing object grouping to a mailing address, they can be considered as follows:
State (= class), city (=instance), and town (= attribute)
For inverter control, available parameters and operation commands are grouped into classes.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-F500, FR-A500