Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21929
  • Release Date : 2018/08/22 16:30
  • Print

I want to synchronize the Z200 and E500.

I want to synchronize speed of the E500 for a new conveyor with the speed of the unit currently using the Z200. How can I do this?
Category : 

Answer

If you are using analog voltage commands, connect the voltage inputs to the FR-E500 and FR-Z200 in parallel to equalize inputs to both units and speeds are synchronized.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-Z200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries