FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Concurrent monitoring of running frequency, output voltage, and output current
FAQ
Concurrent monitoring of running frequency, output voltage, and output current
I want to output signals of the running frequency, output voltage, and output current from the inverter to an external monitoring device simultaneously. How can I do this?
Can I use the plug-in option FR-A5AY to implement this monitoring?
The externally output signals are 4 to 20 mA, 0 to 5 (10) V.
Can I use the plug-in option FR-A5AY to implement this monitoring?
The externally output signals are 4 to 20 mA, 0 to 5 (10) V.
- Category :
Answer
Add an analog output by the FR-A5AY.
Monitor the three output; output AM (0 to 5 (10) V) and optional 4 to 20 mA, and 0 to 5 (10) V.
Monitor the three output; output AM (0 to 5 (10) V) and optional 4 to 20 mA, and 0 to 5 (10) V.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F500, FR-A500