FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > AC reactor and line noise filter wiring
FAQ
AC reactor and line noise filter wiring
I have the following questions about wiring between the AC reactor and line noise filter:
1. Breaker -> AC reactor (FR-BAL) -> line noise filter (FR-BSF01) -> the inverter
2. Breaker -> line noise filter (FR-BSF01) -> AC reactor (FR-BAL) -> the inverter
Which of the above orders is correct?
1. Breaker -> AC reactor (FR-BAL) -> line noise filter (FR-BSF01) -> the inverter
2. Breaker -> line noise filter (FR-BSF01) -> AC reactor (FR-BAL) -> the inverter
Which of the above orders is correct?
- Category :
Answer
Basically, either is OK.
Both orders are electrically identical, but "1" is recommended since it is preferable to place the line noise filter close to the inverter.
If the wiring length between the line noise filter and the inverter is long, the radiation noise from the wiring between them cannot be prevented.
Both orders are electrically identical, but "1" is recommended since it is preferable to place the line noise filter close to the inverter.
If the wiring length between the line noise filter and the inverter is long, the radiation noise from the wiring between them cannot be prevented.
- Product Name
- Inverter, magnet motor drive
- Series
- Others