FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Built-in potentiometer and current input switching control
FAQ
Built-in potentiometer and current input switching control
Can I switch between the operation panel potentiometer and current input from an external source with the FR-E520 series inverter?
- Category :
Answer
For setting the frequency, you cannot switch between the operation panel potentiometer and current input from an external source.
To switch between the external potentiometer and current input, you can use the AU signal input from an external source.
To switch between the external potentiometer and current input, you can use the AU signal input from an external source.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500