FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Magnet motor drive > Motor heat generation
FAQ
Motor heat generation
I use the MM-CF352 (rated current 12.5 A) at around 4 A. (24-hour continuous operation)
The surface temperature is approximately 70 deg C. Is this OK?
The surface temperature is approximately 70 deg C. Is this OK?
- Category :
Answer
The surface temperature of approximately 70?C is OK.
The following shows the MM-CF352 frame temperature for reference.
(Actual temperature rise depends on how the motor is attached.)
- Rated speed (2000 r/min), Under rated load: Around 60 degrees
- Rated speed (2000 r/min), Under no load: Around 30 degrees
If you install the motor where people may touch it, attach a cover to it to prevent the motor from being touched.
The following shows the MM-CF352 frame temperature for reference.
(Actual temperature rise depends on how the motor is attached.)
- Rated speed (2000 r/min), Under rated load: Around 60 degrees
- Rated speed (2000 r/min), Under no load: Around 30 degrees
If you install the motor where people may touch it, attach a cover to it to prevent the motor from being touched.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Motor
- Series
- Magnetic motor drive