FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Can I replace the cooling fan alone?
FAQ
Can I replace the cooling fan alone?
I have purchased the FR-A024 approximately four years ago. The E.FAn error occurred the other day due to blocking by dust. My environment seems not good and the fan does not last long.
If it is possible to replace the fan, I want to have spare fans. As the fan of the FR-E500 is replaceable, does FR-A024 also allow for fan replacement?
If it is possible to replace the fan, I want to have spare fans. As the fan of the FR-E500 is replaceable, does FR-A024 also allow for fan replacement?
- Category :
Answer
The fan of the FR-A024 cannot be replaced by the customer. Mitsubishi Electric System & Service will replace it, so contact us to order it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024