FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Brake resistor
FAQ
Brake resistor
I use an external brake (separate circuit) to stop the motor from high-speed rotation (approximately 40 Hz) and low-speed rotation (approximately 20 Hz).
The inverter coasts to stop at this time. Is the brake resistor necessary?
The inverter coasts to stop at this time. Is the brake resistor necessary?
- Category :
Answer
Connecting the brake resistor allows for quick deceleration because the regenerative power is processed. (The brake torque increases.)
Therefore, when an external brake is used and the inverter coasts to stop, the brake resistor is not necessary.
However, if you are rapidly decelerating the motor from high speed to low speed, the brake resistor may be necessary for this deceleration.
The FR-A500 series with up to 7.5K capacity has a built-in brake resistor.
Therefore, when an external brake is used and the inverter coasts to stop, the brake resistor is not necessary.
However, if you are rapidly decelerating the motor from high speed to low speed, the brake resistor may be necessary for this deceleration.
The FR-A500 series with up to 7.5K capacity has a built-in brake resistor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500, FR-A500