FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > As to batch storing of data file (EcoWebServerIII).
FAQ
As to batch storing of data file (EcoWebServerIII).
Any method for collectively store data files stored in the EcoWebServerIII?
Answer
Using the setting software attached with an EcoWebServerIII (MES3-255C-EN, MES3-255C-DM-EN), it is able to collectively store data per every kind.
Additionally, it is able to automatically transfer files to the FTP server by means of FTP communication.
Refer to the manual for operation / setting.
The manual is downloaded in this site.
Additionally, it is able to automatically transfer files to the FTP server by means of FTP communication.
Refer to the manual for operation / setting.
The manual is downloaded in this site.
- Product Name
- Energy Saving Data Collecting Servers
- Series
- EcoWebServerIII
May I have your opinion?
Related FAQ
- The LED indication of the 7-segment rotates (EcoWebServerIII).
- Cautions for replacing a battery (EcoWebServerIII).
- When displaying current value on EcoWebServerIII, the display goes blank.
- Download of EcoWebServerIII graph data.
- Method for creating a daily/monthly report using logging data (Model: EMU4-LM).