Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22123
  • Release Date : 2018/08/27 16:41
  • Print

As to connecting an Extension Unit for an Insulation Monitor Model (Model: EMU4-LG1-MB).

Is it possible to connect an Energy Measuring Extension Model for Same Voltage System (Model: EMU4-A2), an Energy Measuring Extension Model for Different Voltage System (Model: EMU4-VA2) to the Insulation Monitor Model (Model: EMU4-LG1-MB)?
Category : 

Answer

Connectable.
Provided that it is impossible to extend a measuring circuit for insulation monitoring.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?