Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22126
  • Release Date : 2018/08/27 16:41
  • Print

Setting of "Master / slave setting switch" (Model: EMU4-D65).

An error is indicated immediately after starting the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit.
What kind of causes assumed?
Category : 

Answer

It is assumed that setting of "Master/Slave setting switch" at the bottom of the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit is wrong. Perform settings as below depending on usages.

1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries