FAQ


FAQAbout Products
 - FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Setting of "Master / slave setting switch" (Model: EMU4-D65).
 
FAQ
Setting of "Master / slave setting switch" (Model: EMU4-D65).
      An error is indicated immediately after starting the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit. 
What kind of causes assumed?
  
What kind of causes assumed?
Answer
    It is assumed that setting of "Master/Slave setting switch" at the bottom of the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit is wrong. Perform settings as below depending on usages. 
1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
    1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
- Product Name
 - Energy Measuring Units
 
- Series
 - EcoMonitor Plus