Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22130
  • Release Date : 2018/08/27 16:41
  • Update : 2018/09/07 12:54
  • Print

As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).

Instruct what kind current sensor is usable for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
Category : 

Answer

Refer to the below table as to current sensor usable for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).

*2. It will conform to UL standard, CE marking in combination with the main unit.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?