FAQ


FAQAbout Products

- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).
FAQ
As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).
What happens when the measurement value of the electric energy exceeds 99999.9kWh(MWh)?
Answer
It measures from 0kWh(MWh) after going round.
Integer 4 digits : 9999.98→9999.99→0000.00→0000.01kWh(MWh)
Integer 5 digits : 99999.8→99999.9→00000.0→00000.1kWh(MWh)
Integer 6 digits : 999998→999999→000000→000001kWh
Integer 4 digits : 9999.98→9999.99→0000.00→0000.01kWh(MWh)
Integer 5 digits : 99999.8→99999.9→00000.0→00000.1kWh(MWh)
Integer 6 digits : 999998→999999→000000→000001kWh
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight