FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to using SD memory card at multiple locations.
FAQ
As to using SD memory card at multiple locations.
As to measurements at several points using the EcoMonitorLight, is the number of SD memory card used for the Logging Unit needed for the number of the Logging Unit?
Answer
Setting different logging ID enables that one SD memory card can be used for several Logging Units. Settable logging ID is 1 to 255.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- As to timing for outputting data file into the SD memory card.
- Cautions for replacing a battery (Model: EMU4-LM).
- As to logging after removing an SD memory card.
- As to Zero-Phase Current Transformer (ZCT) usable for the EcoMonitorPlus (Model: EMU4-LG1-MB).
- As to periodic electric energy (EcoMonitorPlus/Light).