Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22133
  • Release Date : 2018/08/27 16:41
  • Print

As to timing for outputting data file into the SD memory card.

When is the time to output data file from EMU4-LM into the SD memory card?
Category : 

Answer

EMU4-LM outputs data file at following timing.

1. When inserting the SD memory card while operating.
2. When power is ON in a state of the SD memory card inserted.
3. At every hour on the hour while operating in a state of the SD memory card inserted.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?