FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to logging period of the optional SD memory card (EMU4-SD2GB).
FAQ
As to logging period of the optional SD memory card (EMU4-SD2GB).
How long is the logging period of the optional SD memory card (EMU4-SD2GB).
Answer
Logging period of the optional SD memory card (EMU4-SD2GB) is according to the logging cycle of detail data and the number of measuring circuits.
* It is the period until capacity of the 2GB SD memory card is exceeded during permanent connection. Data amount depends on the number of characters. It is the logging period where data is output at maximum volume.
* It is the period until capacity of the 2GB SD memory card is exceeded during permanent connection. Data amount depends on the number of characters. It is the logging period where data is output at maximum volume.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
- As to logging period of the internal memory of the main unit.
- As to connecting an Extension Unit for an Insulation Monitor Model (Model: EMU4-LG1-MB).
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- As to required number of Display Unit.