FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to compensation for power failure of Logging Unit for the Energy Measuring Unit.
FAQ
As to compensation for power failure of Logging Unit for the Energy Measuring Unit.
Are setting value, clock and data lost when a power failure occurred in the Logging Unit?
Answer
Since the setting value is stored into nonvolatile memory, it will not be lost.
The clock, logging data and system log data are retained as long as a battery compensating for power failure is valid.
Note that the battery life compensating for power failure is total 1 year (daily average temperature is below 35oC). Battery should be replaced every 3 year.
The clock, logging data and system log data are retained as long as a battery compensating for power failure is valid.
Note that the battery life compensating for power failure is total 1 year (daily average temperature is below 35oC). Battery should be replaced every 3 year.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
- Extension of current sensor cable (EcoMonitorPlus/Light).
- As to changing location of the decimal point and units of the measured value.
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- Extension of cable of the Display Unit (Model: EMU4-D65).