Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22138
  • Release Date : 2018/08/27 16:41
  • Update : 2018/09/07 13:07
  • Print

As to compensation for power failure of Logging Unit for the Energy Measuring Unit.

Are setting value, clock and data lost when a power failure occurred in the Logging Unit?
Category : 

Answer

Since the setting value is stored into nonvolatile memory, it will not be lost.
The clock, logging data and system log data are retained as long as a battery compensating for power failure is valid.
Note that the battery life compensating for power failure is total 1 year (daily average temperature is below 35oC). Battery should be replaced every 3 year.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?