FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to required number of Display Unit.
FAQ
As to required number of Display Unit.
Is the required number of and Display Unit equal to the number of Energy Measuring Unit?
Answer
When reconnecting each unit, customer can use one unit for several purposes. Provided that if it is needed to display the measured value constantly, the number of Display Unit is needed equal to the number of Energy Measuring Unit.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus
May I have your opinion?
Related FAQ
- Cause of "minus" indication for electric power value (EcoMonitorPlus/Light).
- As to connecting an Extension Unit for an Insulation Monitor Model (Model: EMU4-LG1-MB).
- As to logging period of the optional SD memory card (EMU4-SD2GB).
- As to compensation for power failure (EcoMonitorPlus/Light).
- Cautions for replacing a battery (Model: EMU4-LM).