FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > MEASURE LED not blink (EcoMonitorPlus).
FAQ
MEASURE LED not blink (EcoMonitorPlus).
What cause assumed for no blink of MEASURE LED?
Answer
MEASURE LED lights while measuring electric power over 0.4% of the total load power. Check below points:
1. Is voltage wiring connected?
2. Are the transfix direction of current sensor, connection of k, l terminals reversed?
1. Is voltage wiring connected?
2. Are the transfix direction of current sensor, connection of k, l terminals reversed?
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus