Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22144
  • Release Date : 2018/08/27 16:41
  • Print

MEASURE LED not blink (EcoMonitorPlus).

What cause assumed for no blink of MEASURE LED?
Category : 

Answer

MEASURE LED lights while measuring electric power over 0.4% of the total load power. Check below points:
1. Is voltage wiring connected?
2. Are the transfix direction of current sensor, connection of k, l terminals reversed?
Product Name
Energy Measuring Units
Series
EcoMonitor Plus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?