FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Disable an alarm for motor starting current (ME96SS series).
FAQ
Disable an alarm for motor starting current (ME96SS series).
Is it possible to stop the alarm for motor starting current in the motor circuit?
Answer
This model has “Motor Starting Current Mask Function”. This function stops the alarm output and updating of the maximum values during the setting time when a current value exceeds the threshold.
(Please refer to the Set-up menu 5 “Motor starting current delay time” of the section 3 in the User’s Manual.)
(Please refer to the Set-up menu 5 “Motor starting current delay time” of the section 3 in the User’s Manual.)
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series