FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > How to use the "S/S" terminal
FAQ
How to use the "S/S" terminal
How do you use the "S/S" terminal of the MELSEC-F series?
Answer
The "S/S" terminal is used to switch the input type (sink input and source input).
For the source input, connect the "S/S" terminal to the "0V" terminal, and short-circuit between the "24V" terminal and the "- input terminal: X□□□" to turn on the input.
For the sink input, connect the "S/S" terminal to the "24V" terminal, and short-circuit between the "0V" terminal and the "- input terminal: X□□□" to turn on the input.
For the source input, connect the "S/S" terminal to the "0V" terminal, and short-circuit between the "24V" terminal and the "- input terminal: X□□□" to turn on the input.
For the sink input, connect the "S/S" terminal to the "24V" terminal, and short-circuit between the "0V" terminal and the "- input terminal: X□□□" to turn on the input.
- Product Name
- FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
- Product Category
- Main unit, I/O Extension
- Series
- MELSEC-F series