FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the type of Ethernet connection cable
FAQ
Regarding the type of Ethernet connection cable
Which type of Ethernet connection cable should be used to connect FX5 CPU module and GX Works3(Computer)?
Answer
Ethernet standard-compatible cable, category 5 or higher (STP cable) can be used.
*Straight cable can be used.
When connecting directly to the computer, cross cable can also be used.
*Straight cable can be used.
When connecting directly to the computer, cross cable can also be used.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series