Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22311
  • Release Date : 2018/08/30 13:55
  • Update : 2023/02/13 15:34
  • Print

Regarding the maximum number of channels of high-speed counters

Up to how many CHs can the FX5 CPU module's high-speed counter be controlled?
Category : 

Answer

The FX5 CPU module's built-in high-speed counter can control up to 8CH.
Up to 16CH can be controlled by adding 4 modules of FX5-16ET/E□-H (high-speed pulse I/O module) to the FX5U/FX5UC/FX5UJ CPU module.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, High-Speed Counter
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries