FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the settings of built-in analog function of FX5U CPU module
FAQ
Regarding the settings of built-in analog function of FX5U CPU module
Are there any required settings for using the built-in analog function?
Answer
The settings can be done using the parameter settings of GX Works3 or by settings the special relay/special registers.
For further details please refer to MELSEC iQ-F FX5 User's Manual (CPU Module Built-In Analog/Expansion-Adapter).
For further details please refer to MELSEC iQ-F FX5 User's Manual (CPU Module Built-In Analog/Expansion-Adapter).
- Product Name
- FX5U
- Product Category
- CPU Module, Analog
- Series
- MELSEC iQ-F Series