FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the system configuration of FX5-CCL-MS with FX5 CPU module
FAQ
Regarding the system configuration of FX5-CCL-MS with FX5 CPU module
How many FX5-CCL-MS can be connected to FX5 CPU module?
Answer
A total of two FX5-CCL-MS (CC-Link system master/intelligent device) can be connected: one as a master station and one as an intelligent device station.
- Product Name
- FX5-CCL-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series