FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the maximum number of connections for MODBUS communication
FAQ
Regarding the maximum number of connections for MODBUS communication
When MODBUS communication is used as master station, how many slave stations can be connected?
Answer
32 stations can be connected when RS-485 port is used and only 1 station can be connected when RS-232 port is used.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series