FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > GX Works2's USB driver installation procedure
FAQ
GX Works2's USB driver installation procedure
Is the USB driver installed along with the installation of GX Works2?
- Category :
Answer
The USB driver is not installed.
The driver needs to be separately installed before the first connection to a CPU module.
The driver needs to be separately installed before the first connection to a CPU module.
- Product Name
- MELSEC-Q Series
- Series
- Software Package (GPP function)