FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Error code "4100" in QCPU
FAQ
Error code "4100" in QCPU
The error code "4100" is displayed on QCPU.
The instruction in which the error occurs is [D/ D6270 D6268 D6268]. Are there any remedies?
The instruction in which the error occurs is [D/ D6270 D6268 D6268]. Are there any remedies?
- Category :
Answer
The error code "4100" is "OPERATION ERROR".
The error occurs when a number is divided by 0 (Divisor D6268 value is 0).
Make modifications so that the divisor is other than 0 when it is executed.
The error occurs when a number is divided by 0 (Divisor D6268 value is 0).
Make modifications so that the divisor is other than 0 when it is executed.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)