FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > VxWorks
FAQ
VxWorks
What kind of operating system is VxWorks, which is installed in C Controller module?
- Category :
Answer
It is an embedded RTOS (real-time OS) developed by Wind River, which is proven worldwide as reliable and stable.
The version of the operation system installed in Q06CCPU-V is 5.4 and its development environment is Tornado 2.1.
The version of the operation system installed in Q12DCCPU-V is 6.4 and its development environment is CW Workbench or Wind River Workbench 2.6.1.
The version of the operation system installed in Q06CCPU-V is 5.4 and its development environment is Tornado 2.1.
The version of the operation system installed in Q12DCCPU-V is 6.4 and its development environment is CW Workbench or Wind River Workbench 2.6.1.
- Product Name
- MELSEC-Q Series
- Series
- CPU