FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Network No., Group No., and Station No. in Network Parameter
FAQ
Network No., Group No., and Station No. in Network Parameter
In the parameter setting of Ethernet interface module (QJ71E71-100/B2/B5), what do Network No., Group No., and Station No.,
which are in Ethernet/CC IE/MELSECNET cards of Network Parameter, mean?
which are in Ethernet/CC IE/MELSECNET cards of Network Parameter, mean?
- Category :
Answer
- Network No. is a number assigned to identify each network when multiple networks are configured.
Each network No. must be unique.
- Group No. is a number assigned to group stations in a network.
Transient transmission allows data to be transmitted to multiple stations in the same group.
- Station No. is a number assigned to identify each network module connected to a network.
The station No. of each network module must be unique in a network.
Each network No. must be unique.
- Group No. is a number assigned to group stations in a network.
Transient transmission allows data to be transmitted to multiple stations in the same group.
- Station No. is a number assigned to identify each network module connected to a network.
The station No. of each network module must be unique in a network.
- Product Name
- MELSEC-Q Series
- Series
- Ethernet Interface Module