FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Error code "2200" in the universal model QCPU
FAQ
Error code "2200" in the universal model QCPU
The error code "2200" has occurred in a universal model QCPU module. Are there any remedies?
- Category :
Answer
The error code "2200" is "MISSING PARA.".
The cause of the error is that a parameter file does not exist in all drives where parameters will be valid.
As a remedy, write a parameter file into a PLC drive to be valid.
The cause of the error is that a parameter file does not exist in all drives where parameters will be valid.
As a remedy, write a parameter file into a PLC drive to be valid.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)