FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Error code "2100" in QCPU
FAQ
Error code "2100" in QCPU
The error code "2100" has occurred in QCPU. Are there any remedies?
- Category :
Answer
The error code "2100" is "SP.UNIT LAY ERR.". This error may be caused by one of the following factors.
(1) In the I/O assignment setting of the PLC parameter, an I/O module is assigned as "Intelli."
(intelligent function module), or vice versa.
(2) In the I/O assignment setting of the PLC parameter, the CPU module is assigned as another type of module or "Empty",
or vice versa.
(3) In the I/O assignment setting of the PLC parameter, the number of points assigned to the intelligent function module is less
than the number of points of the connected module.
As a remedy, set the I/O assignment again in the I/O assignment setting of the PLC parameter, so that the setting matches with
the mounted status of the intelligent function module or the CPU module.
(1) In the I/O assignment setting of the PLC parameter, an I/O module is assigned as "Intelli."
(intelligent function module), or vice versa.
(2) In the I/O assignment setting of the PLC parameter, the CPU module is assigned as another type of module or "Empty",
or vice versa.
(3) In the I/O assignment setting of the PLC parameter, the number of points assigned to the intelligent function module is less
than the number of points of the connected module.
As a remedy, set the I/O assignment again in the I/O assignment setting of the PLC parameter, so that the setting matches with
the mounted status of the intelligent function module or the CPU module.
- Product Name
- MELSEC-Q Series
- Series
- CPU