FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Parameter settings required to use the MODBUS(R) interface module as a slave station
FAQ
Parameter settings required to use the MODBUS(R) interface module as a slave station
Is it necessary to set parameters when the MODBUS(R) interface module QJ71MB91/QJ71MT91 is used as a slave station?
- Category :
Answer
If preset initial values are used, parameters do not need setting.
If changing the basic parameter or MODBUS(R) device assignment parameter, use a sequence program, GX Works2, or GX Configurator-MB to change it.
If changing the basic parameter or MODBUS(R) device assignment parameter, use a sequence program, GX Works2, or GX Configurator-MB to change it.
- Product Name
- MELSEC-Q Series
- Series
- MODBUS