FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Detecting the connection between a built-in Ethernet port QCPU and hub
FAQ
Detecting the connection between a built-in Ethernet port QCPU and hub
How can I check the connection to a hub with a built-in Ethernet port QCPU?
- Category :
Answer
You can check the connection to the hub with bit 10 of the special register SD1288. When bit 10 of the SD1288 is on, the QCPU is in connection with the hub.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)