FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Versions of built-in Ethernet port LCPU compatible with SNTP function
FAQ
Versions of built-in Ethernet port LCPU compatible with SNTP function
I would like to use the time setting function (SNTP client) of the L series CPU with built-in Ethernet port to synchronize clocks. Are there any restrictions on the model or version of CPU?
- Category :
Answer
The initial version and subsequent versions of L series CPU support the SNTP function.
- Product Name
- MELSEC-L Series
- Series
- L Series